Add retentivity storage to the project

Add retentivity storage to the project

Add retentivity storage to the project to make changes persistent.
  1. In
    Project view
    , right-click
    Retentivity
    and select
    New
    Retentivity storage
    .
  2. In
    Properties
    , next to
    Nodes
    , select
    Add
    .
  3. Create a dynamic link between
    Node1
    and
    ProjectName
    Security
    Users
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal