Create an alarm grid

Create an alarm grid

Add a preconfigured alarm grid.
  1. Add a preconfigured widget (type):
    1. In the toolbar, select
      Template Libraries
      .
    2. In
      Libraries
      , search for
      Alarm Grid
      .
    3. Under
      Components
      , drag
      Alarm Grid
      onto
      UI
      in
      Project view
      .
  2. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    AlarmGrid
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal