Add a screen instance

Add a screen instance

Create an instance of a screen type and modify the screen instance properties.
Prerequisites
  1. Right-click a node to contain the screen object and select
    New
    Screens
    ScreenName
    .
    The screen object instance appears under the node and inherits the properties of the screen type.
  2. (optional) In
    Properties
    , set the screen instance properties.
    For more information, hover-over the properties.
  3. (optional) Add objects to the screen instance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal