Navigate nodes

Navigate project content in
Project view
.
  • Do any of the following:
  • Select any node in
    Project view
    and start typing the name of the node to find.
    The matching note is selected.
    TIP: The nodes are searched downward from the currently selected node. If there are no matches, the search continues from the first node to the currently selected node.
  • Expand the selected node by pressing
    Right arrow
    .
  • Collapse the selected node by pressing
    Left arrow
    .
  • Select the lower node by pressing
    Down arrow
    .
  • Select the upper node by pressing
    Up arrow
    .
  • Select the previously selected node by selecting
    Navigate backward
    .
  • Select the most recent node by selecting
    Navigate forward
    .
  • Right-click the root project node and then select
    Collapse all
    to collapse all nodes for easier navigation.
  • Divide
    Project view
    into two areas that you can scroll separately. Select 
    Split project view
    to divide the view. Select 
    Split project view
    again to remove the division in the view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal