Create a variable

Create a variable

Create a variable in
Project view
.
  1. In
    Project view
    , select the folder or object to contain the variable.
  2. In the
    Project view
    toolbar, select
    Add
    Add new
    and then select
    Variable
    .
  3. (optional) To change the variable data type, in
    Properties
    , next to the variable name, select the existing data type and then select another data type.
    TIP:
    If you do not see the required option, select
    Show all
    . Start typing to select the item to find.
    To define an array, select
    Array
    and then enter the array dimensions. Enter
    0
    to create an unconstrained array.
  4. In
    Properties
    , select
    Edit
    and enter a value for the variable or create a dynamic link.
    If you edit an array variable value, the Array editor displays. For more information, see Array editor.
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal