Remove the unit of measure from a variable

Remove the unit of measure from a variable

Remove the unit of measure for a variable to no longer have the value for that variable appear in that unit of measure.
  1. In
    Project view
    , select a variable.
  2. In
    Properties
    , select the unit of measurement in the value of the variable.
  3. Select
    <None>
    and then choose
    Select
    .
The unit of measure is removed from the variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal