Zoom in and zoom out a trend chart

Zoom the X and Y axes of a trend chart to focus on specific data. Zoom in and zoom out the trend chart axes together or separately.
  • To zoom in and zoom out the X and Y axes
  • Use the pinch-to-zoom gesture.
  • Place the mouse pointer in the area of interest of the trend chart and scroll forward or backward.
  • Select the trend chart and select
    +
    or
    -
    .
  • To zoom in and zoom out only the X-axis
  • Place the mouse pointer anywhere in the trend chart, hold
    Ctrl
    , and then scroll up or down.
  • To zoom in and zoom out only the Y-axis
  • Place the mouse pointer anywhere in the trend chart, hold
    Alt
    , and then scroll up or down.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal