Debug NetLogic remotely

Debug NetLogic remotely

With Visual Studio, you can remotely debug a runtime NetLogic on Windows systems.
TIP: Remote debugging is not possible on HMIs for security reasons. For more information about remote debugging, see Remote debugging - Visual Studio (Windows) | Microsoft Learn.
To debug NetLogic locally, see Debug NetLogic locally.
Prerequisites
  • On the development machine, download Visual Studio and set as the default code editor. See Set the default code editor.
  • Verify that the client machine and the development machine are connected to the same network.
  1. To debug runtime NetLogic remotely
  2. Configure the remote Windows machine as a target in
    FactoryTalk Optix Studio
    . See Add a client device.
  3. Stop the debugger and application runtime and then edit the code.
    TIP: To stop the remote debugging process, close the Remote Debugger desktop application or stop debugging in Visual Studio.
  4. Repeat 3.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal