- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Sessions and locales
- Object and variable references
- Extending projects
- NetLogic
- NetLogic tutorial
Change the unit of measure for a variable
Change the unit of measure for a variable that displays at runtime.
- InProject view, select a variable.
- InProperties, select the unit of measurement in the value of the variable.
- Select the unit of measure for the variable value and chooseSelect.
The unit of measure appears in the value for the variable.
Provide Feedback