Array editor

Array editor

Use the array editor to modify the values of array variables.
Array editor
Array editor items
Item
Name
Description
1
Add
Add
Adds a cell to an unconstrained array.
2
Delete
Removes a cell from an unconstrained array.
3
Array cells column
Lists array cells.
4
Array values column
Lists editable array cell values.
TIP: If the array lists colors, you can select the color preview to open the color selector.
5
Apply
button
Applies changes to the array values and closes the editor.
6
Cancel
button
Cancels changes to the array values and closes the editor.
7
Open in tab
button
Opens the array editor in the central pane.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal