Scroll view

Scroll view

Panel that can scroll to display content larger than the panel size.

Operation

Scroll view supports:
  • Touch and multitouch gestures, such as pan or pinch-to-zoom.
  • Keyboard and mouse operation, such as the
    Ctrl
    Scroll wheel
    combination to zoom-in or zoom-out.

Use case

Display overview information, drawings, or other items that are larger than the main application container.

Example

Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal