Configure a presentation engine

Configure a presentation engine

Add a native presentation engine or a web presentation engine to your project.
TIP: Each project can contain a single native presentation engine and a single web presentation engine.
  1. In
    Project view
    , right-click a window object.
  2. Select one of the following options:
    • To create a native presentation engine, select
      New
      Native presentation engine
      .
    • To create a web presentation engine, select
      New
      Web presentation engine
      .
  3. (optional) In
    Properties
    , edit the presentation engine options.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal