Debug NetLogic locally

Debug NetLogic locally

Identify, investigate, and fix issues with NetLogic code by locally using Visual Studio or Visual Studio Code.
To debug NetLogic remotely, see Debug NetLogic remotely.
TIP: NetLogic errors are reported at runtime in the
FactoryTalk Optix Studio
log panel. NetLogic runtime errors are reported in the tab of the target on which the application runs (for example,
Emulator Output
). The design-time NetLogic errors are reported in the
Output
tab.
For more information, refer to the external code editor documentation.
Prerequisites
  1. To debug NetLogic
  2. From the main toolbar, select
    Open .NET Solution
    .
    The default external code editor opens.
    TIP: Rockwell Automation recommends using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor.
  3. Debug either:
    • Runtime NetLogic. In the external code editor, debug
      FTOptixRuntime
      and in
      FactoryTalk Optix Studio
      , select
      Run
      .
      TIP: You can run the project on the Emulator target for debugging.
    • Design-time NetLogic. In the external code editor, debug
      FTOptixStudio
      and in
      FactoryTalk Optix Studio
      , right-click a NetLogic and select a method to execute.
  4. Stop the debugger and application runtime and then edit the code.
  5. Repeat 2.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal