Project Development

Application Code Manager
organizes components into projects. Use one of the following methods to create projects:
  • Add a project using the
    Object Configuration Wizard
    .
  • Create a project from an existing project.
  • Import a project using ACM or ACM Console.
Once a project is created, add objects for your application, such as:
  • Historian objects
  • HMI objects
  • Alarm objects
  • Batch objects
  • Controllers and controller objects
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal