Add an Alarm Group subobject

FactoryTalk® Alarms and Events
objects have subobjects that represent the Alarm Groups configured in the FTAE system. In FactoryTalk Alarms and Events, alarms can be assigned to groups. A group represents a set of alarms with a common association. An alarm group can contain other groups organized in a hierarchy (FTAE only supports to five levels deep).
To add an Alarm Group subobject
  1. In the
    System View
    pane, expand
    HMI
    , expand
    Alarms
    and then click the
    FactoryTalk Alarms and Events
    object to which the subobject will be added.
  2. In the object parameters pane, select the
    Alarm Group
    tab.
  3. Right-click in the white space below the objects shown in the tab. Click
    Add New
    .
    Repeat this step to add all of the Alarm Group that requires configuration.
  4. An alarm group hierarchy is achieved by associating one alarm group to another using the ParentAlarmGroupID parameter.
  5. Click the appropriate column and modify the parameters as needed.
  6. Click
    Apply Changes
    to save the parameter configuration.
Group subobjects
Group subobjects into categories based on the data columns.
  • Double-clicking a column heading updates the display in the parameters tab to group items with the same value together.
  • Right-click anywhere in the parameters tab and select
    Reset Grouping
    to return to the default display.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal