Find an object

Use the
Find
dialog
to search for an object or a library in the
Class View
pane, contents in the
Preview
tree, or a library in the
Registered Libraries
tree.
To find an object
  1. On the toolbar, select
    EDIT > Find
    .
  2. In
    Find what
    , enter the name of an object.
  3. In
    Look in
    , select
    Class View
    ,
    Preview
    , or
    Registered Libraries
    .
  4. (optional) In
    Find Options
    , select the checkboxes of
    Match case
    and
    Match whole word
    .
  5. Select
    Find Next
    or
    Find Previous
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal