Add a Historian object

Add a Historian object to the project to support integration of Historian data.
To add a Historian object
  1. In the
    System View
    pane, expand
    Historian
    , right-click
    ScanClass
    and then click
    Add
    .
    The
    Object Configuration Wizard
    appears.
  2. Under
    Select a library
    in the
    Solution
    column, click the + symbol to expand a library category and display the Historian libraries registered in the connected ACM database.
  3. Click a Historian library, the row highlights to indicate that it is selected. Click
    Next
    .
  4. In
    Name
    , type a unique name for the Historian object and then click
    Finish
    .
    The Historian object is added to the
    System View
    pane as a child object of
    ScanClass
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal