Add an HMI object

Add an HMI object to support
FactoryTalk View SE
,
FactoryTalk View ME
, or Alarms displays in the project.
To add an HMI object
  1. In the
    System View
    pane, expand
    HMI
    to see the HMI categories.
    • To add a
      FactoryTalk View SE
      or
      FactoryTalk View ME
      HMI object, right-click
      Displays
      and then click
      Add
      .
    • To add a
      FactoryTalk Alarms and Events
      object or
      FactoryTalk View ME
      alarm object, right-click
      Alarms
      and then click
      Add
      .
      The
      Object Configuration Wizard
      appears.
  2. Under
    Select a library
    in the
    Solution
    column, click the + symbol to expand a library category and display the libraries registered in the connected ACM database.
  3. Click a library, the row highlights to indicate that it is selected. Click
    Next
    .
  4. In
    Name
    , type a unique name for the object and then click
    Finish
    .
    The object is added to the
    System View
    pane as a child object of the HMI category.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal