Create a project from a project

Use an existing project in the ACM database as the basis for a project if the projects use the same components and libraries.
If the project is in a different ACM database, such as one from another installation, you must connect to that database, export the project, and then import it to the current database.
To create a project from an existing project
  1. Click
    File > New > Project from Existing Project
    . The
    New Project Wizard
    is displayed.
  2. On the
    Create a new Project from an existing Project
    page, in
    From Project
    , select the project name from the list.
  3. In
    New Name
    , type a name for the new project.
  4. (optional) In
    New Description
    , type a description of the new project.
  5. Click
    OK
    .
    The new project appears highlighted in the
    System View
    pane.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal