FTAE Alarm Group parameters
The
Alarm Group
tab displays a columnar grid of the parameters defined for the alarm groups of the FactoryTalk Alarms and Events
object.This table describes the parameters in the
Alarm Group
tab.Parameter | Description |
|---|---|
Name | The name of the subobject representing the Alarm Group (not the name to be used
in the FTAE system). Through name formatting, a unique subobject name is built up
from the AlarmGroup and ParentAlarmGroupID parameters. |
AlarmGroupID | Each AlarmGroupID must be unique (0 is reserved for the FTAETagServer ID). |
ParentAlarmGroupID | The ParentAlarmGroupID determines the alarm group hierarchy (Default: 0 = FTAETagServer ID). |
AlarmGroup | The alarm group name that will be created in the FTAE system and assigned to FTAE alarm tag objects that reference it. |
SubObject Description | Provides a unique description of the alarm group subobject. |
Provide Feedback