HMI Display parameters

The
Display
tab displays a columnar grid of the parameters defined for the displays of the
FactoryTalk View
object.
This table describes the parameters in the
Displays
tab.
Parameter
Description
Name
The name of the display. Double-click to configure a unique name for the display.
DisplayTitle
Specifies the content of the display title bar.
DisplayLeft
Sets the left edge of a display to the number of units specified from the left edge of the screen.
DisplayTop
Sets the top edge of a display to the number of units specified from the top edge of the screen.
DisplayWidth
Sets the width of a display.
DisplayHeight
Sets the height of a display.
DisplayBackColor
Sets the background color of the display.
DisplaySecurity
Identifies the security class of the screen.
UpdateRate
Defines the amount of time to update a display in response to an event. Default setting is 1.0 seconds. For best performance, set to .1 seconds.
LeftIndexMax
Identifies the maximum number of entries in the left index.
VBAProjectObject
Adds a VBA item to the
FactoryTalk View SE
display. Click the ellipsis (...) button to select a VBA item.
SubObject Description
Provides a unique description of the display subobject.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal