Create a project
Create a project when the new project is not similar to existing projects.
To create a project
- ClickFile > New > Project. TheObject Configuration Wizardis displayed.
- On theSelect a librarypage, click the + symbol to expand the library category and display the libraries registered in the connected ACM database.
- Click a library to select it and then clickNext.
- If the library contains a library link, click theLinked Librariestab.
- Click the link and choose how to instantiate the linked library, select either:
- Create New Instance. To create an instance of the library the link is attached to.
- Link to Existing Instance. To link to a library instance of the target library that has already been created.
- Enter a unique name in theNamefield. Enter a description in theDescriptionfield and clickFinish.The new project appears highlighted in theSystem Viewpane.
Provide Feedback