Add a Display subobject
FactoryTalk View
objects have subobjects that represent the display types
configured. A FactoryTalk View
graphic display represents a run-time operator’s
view of plant activity. A graphic display can show system or process data, and provide an
operator with ways to write values to external devices such as programmable controllers.To add a Display subobject
- In theSystem Viewpane, expandHMI, expandDisplaysand then click theFactoryTalk Viewobject to which the subobject will be added.
- In the object parameters pane, select theDisplaystab.
- Right-click in the white space below the objects shown in the tab. ClickAdd New.Repeat this step to add all of the Displays that require configuration.
- Click the appropriate column and modify the parameters as needed.
- ClickApply Changesto save the parameter configuration.
Group subobjects
Group subobjects into categories based on the data columns.
- Double-clicking a column heading updates the display in the parameters tab to group items with the same value together.
- Right-click anywhere in the parameters tab and selectReset Groupingto return to the default display.
Provide Feedback