Add a Historian subobject

Historian objects have subobjects that represent the point types configured. A FactoryTalk Historian point is the basic building block for controlling data flow to and from the FactoryTalk Historian SE server. A single point is configured for each measurement value that needs archiving.
To add a Historian subobject
  1. In the
    System View
    pane, expand
    Historian
    , expand
    ScanClass
    and then click the Historian object to which the subobject will be added.
  2. In the object parameters pane, select the Point Type tab.
  3. Right-click in the white space below the objects shown in the tab. Click
    Add New
    .
    Repeat this step to add all of the points that require configuration.
  4. Click the appropriate column and modify the parameters as needed.
  5. Click
    Apply Changes
    to save the parameter configuration.
Group subobjects
Group subobjects into categories based on the data columns.
  • Double-clicking a column heading updates the display in the parameters tab to group items with the same value together.
  • Right-click anywhere in the parameters tab and select
    Reset Grouping
    to return to the default display.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal