Arrange graphic objects
After you draw or paste a graphic object, you can move the object around and arrange it using the menu options on the
Arrange
menu or the toolbar.You can:
- Combine several objects into a group that behaves as a single object
- Ungroup a group object, dividing it into its component parts
- Stack objects by moving them in front of or behind other objects
- Align objects with each other vertically or horizontally
- Space objects vertically or horizontally
- Flip objects and groups horizontally or vertically
- Rotate a graphic object or a group
- Lock a graphic object or a group into position
Provide Feedback