Select a graphic object that is behind another object
You can select a graphic object that is behind another object without bringing it to the front.
To select a graphic object that is behind another object
- Click the top object, and then click the top object again.TIP:You can also select the object that is behind another object in theObject Explorer. In theObject Explorer, objects are listed front to back.You can use the checkbox in front of a graphic object in theObject Explorerto show or hide the object on the graphic display.
Provide Feedback