Select a graphic object within a group

You can select a graphic object within a group without ungrouping the objects.
To select a graphic object within a group
  1. Double-click the group to put the group in edit mode.
  2. Do one of the following:
    • Click the object on the graphic display
    • In the
      Object Explorer
      , click the + sign next to a group and click the object in the
      Object Explorer
      . Objects are listed front to back.
      TIP:
      You can use the
      Object Explorer
      to select the objects out of a group.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal