Show or hide a graphic object on a graphic display

You can use the checkbox in front of a graphic object in the
Object Explorer
to show or hide the object on the graphic display.
To show or hide a graphic object on a graphic display
  • In the
    Object Explorer
    , select the checkbox in front of the object you want to show, or clear the checkbox in front of the object you want to hide.
    TIP:
    • By default, all checkboxes in the
      Object Explorer
      are selected and all objects are shown on the graphic display.
    • If you select or clear the checkbox in front of a group in the
      Object Explorer
      , all objects in the group are shown or hidden on the graphic display. If you select or clear the checkbox in front of the root node,
      Display
      in the
      Object Explorer
      , all the objects on the graphic display are shown or hidden.
    • At runtime, the visibility state of a graphic object depends on the expression. The
      Object Explorer
      visibility state of a graphic object has no effect on the default visibility state of the object at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal