Space graphic objects

Use the
Space Vertical
and
Space Horizontal
options on the
Arrange
menu to move the selected objects so there is an equal amount of space between them. You must select at least three objects to use either of these commands.
To space graphic objects equidistant from each other
  1. Select at least three objects.
  2. From the
    Arrange
    menu, select the spacing option you want to apply.
    TIP:
    To arrange objects in a column, arrange them roughly, select them, and use
    Align Center
    and then
    Space Vertical
    to arrange them exactly.
    For a horizontal line, use
    Align Middle
    and then
    Space Horizontal
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal