Align graphic objects
Use the
Align
options on the Arrange
menu to position selected objects so that they line up with each other and the grid. Final positioning depends on the commands used.To align graphic objects
- Select the objects you want to align.
- From theArrangemenu, select the align option you want to apply to the selected objects.TIP:You can also align objects using theAlignmenttoolbar. To open theAlignmenttoolbar, from theViewmenu, selectToolbars > Alignment Toolbar.
Provide Feedback