Send a graphic object to the back
Graphic objects can be stacked on top of each other in a graphic display. Use the
Send to Back
option on the Arrange
menu to move the selected object to the bottom of the stack.To send a graphic object to the back
- Select the object.
- From theArrangemenu, selectSend to Back.
You can select several objects or groups of objects with a selection border and move them simultaneously as a single object.
Provide Feedback