Bring a graphic object to the front
Graphic objects can be stacked on top of each other in a graphic display. Use the
Bring to Front
option on the Arrange
menu to move the selected object to the top of the stack.To bring a graphic object to the front
- Select the object.
- From theArrangemenu, selectBring to Front.
You can select several objects or groups of objects with a selection border and move them simultaneously as a single object.
Provide Feedback