Drag a graphic object with a mouse

You may need drag a graphic object.
To drag a graphic object with mouse
  1. Select the object.
  2. Place the pointer on the object, not on its edge or handle.
  3. Press the left mouse button and drag the object to its new location.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal