Resize a graphic object in small increments
Use the
Shift
key with the arrow keys to resize objects in small increments.To resize a graphic object in small increments
- Select the object. Handles appear around it.
- Place the pointer on one of the handles. A double arrow appears.
- Press theShiftkey and an arrow key until the object is the desired size.TIP:You can also resize a graphic object by editing itsHeightandWidthproperties in theProperty Panel.You can resize multiple objects to the same size by selecting them and editing theirHeightandWidthproperties in theShared Propertiespanel.
Provide Feedback