Resize a graphic object using a mouse
You can use a mouse to resize all graphic objects.
To resize a graphic object using a mouse
- Select the object. Handles appear around it.
- Place the pointer on one of the handles. A double arrow appears.
- Drag the handle until the object is the desired size.TIP:
- Drag a side handle to change width or height or a corner handle to change both.
- For perfect circles and squares pressCtrlas you drag a corner handle with the mouse.
- To maintain the aspect ratio (width/height), pressShiftas you drag a corner handle with the mouse.
Provide Feedback