Flip a drawing object

Use the
Flip Vertical
or
Flip Horizontal
options on the
Arrange
menu to move a drawing object so its new position is the reverse of its original position. You can flip all simple drawing objects (except text, panels, and images) and groups.
To flip a drawing object
  1. Select the object you want to reposition.
  2. From the
    Arrange
    menu, select the
    Flip Vertical
    or
    Flip Horizontal
    option.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal