Group graphic objects

Use the
Group
option on the
Arrange
menu to combine selected graphic objects into a group.
To group graphic objects
  1. Select the objects to be grouped.
  2. From the
    Arrange
    menu, select
    Group
    .
    TIP:
    To edit a group, you can double click the group and select individual objects to edit within that group, or use the
    Object Explorer
    . You do not have to ungroup to edit the constituent objects in a group.
    The handles around each object are replaced by a single set of handles around the group. You can use these handles to resize the group, just as you resize a single object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal