Agent Groups
FactoryTalk AssetCentre Agent Groups is a plug-in that helps you manage the agents into groups. With this plug-in, the agent computers that are connected to the same FactoryTalk AssetCentre Server do not need to have the same configuration. You can use agents in the local agent group or assign tasks to a remote agent group that is in another FactoryTalk Directory. This plug-in allows you to:
- Create agent groups, assign agent computers to the agent groups, and identify an agent group for an asset
- Assign backup and compare schedule tasks on an asset to the agent computers that belong to the asset’s agent group
- Monitor the status of agent computers in theAgent Statuspane, theAgent Group Creationand Agent Assignmentpane, and theAssets per Agent Grouppane.
Activation is required for Agent Groups. The number of agent groups that can be managed is determined by what FactoryTalk capacities you have purchased.
Provide Feedback