View Agent status for searches
How do I open the Agent status for searches pane?
- If you are not in it, enter Design mode.
- On theMenu bar, clickView > Agent Groups(or click theAgent Groupsbutton).
- On theAgent Groupstoolbar, click
.
Agent status for searches shows the status for the scheduled search assigned to an agent computer or waiting for interface. If one scheduled search task completed, it will disappear from Agent status for searches.
Agent status refreshes when a running schedule status changed or a new scheduled search started. The last refresh time shows on the upper right corner of the status pane.
TIP:
Use
Agent status for searches
to view the status for the scheduled searches assigned to an agent computer or waiting for interface.Provide Feedback