Scheduled asset status definitions
These status messages are shown next to assets in a schedule (in the lower left pane of the
Schedules
tab) while the schedule is running.This status | Means |
|---|---|
User Disabled | The user has disabled the asset from participating in the schedule. |
Waiting For Interface | The task is waiting for an available agent machine to perform the operation. |
Loading Agent | The agent computer is loading the agent software. This status appears only briefly. |
Loading Data | The agent computer is loading the necessary data to execute the operation (for example, getting a copy of the master file from Archive). This status appears only briefly. |
Running | The task is currently being executed. |
Stopping | The system is waiting for the agent computer to acknowledge a stop command for the operation. This status appears only briefly. |
Unloading Agent | The task has been completed and the agent computer is unloading the agent software. |
Task Done, result string | The task has been completed. The result string (indicating success or failure) appears in the status message. |
Wait For Retry | The operation has failed and has entered a retry state. |
Unloading and Waiting For Retry | The operation has failed and the agent computer is unloading the agent software. This status appears only briefly. |
Connecting to Controller | An agent computer has been assigned and is establishing a connection. |
Change detect in process | A change was detected and the log entries from the controller are being collected. |
Communication error - retrying | Connection to the physical device failed. A message is generated in the Event Log if communication had previously been established. The agent computer continues to retry the scheduled operation. |
Provide Feedback