View Agent status for schedules
How do I open the Agent status for schedules pane?
- If you are not in it, enter Design mode.
- On theMenu bar, clickView > Agent Groups(or click theAgent Groupsbutton).
- On theAgent Groupstoolbar, click
.
Agent status for schedules shows status for the schedules assigned to an agent computer or waiting for interface. If one schedule task completed, it will disappear from Agent status for schedules.
Agent status refreshes when a running schedule status changed or a new schedule started. The last refresh time shows on the up-right corner of the status pane.
TIP:
Use
Agent status for schedules
to view the status for the schedules assigned to an agent computer or waiting for interface.Provide Feedback