About the column headings of Agent status for schedules

The following table shows the column headings of Agent status for schedules and their meanings.
Column heading
Description
Filter row
The filter row below the column headings allows you to filter schedules by column or column entry to show only those schedule definitions you want to view.
Agent Computer Name
The name of the agent computer that executes the schedule task.
Agent Group Name
The identified agent group of the asset for which the schedule was originally created.
Schedule Name
The name of the schedule.
Schedule Location
The asset for which the schedule was originally created. This could be a scheduled container that includes other assets or an individual asset for which you are creating a schedule.
Operation
The type of operation that is scheduled (for example, Backup, Backup and Compare, or Change Detect).
Task State
The schedule task state (for example, Loading Agent, Loading Data, Running or Waiting For Interface, etc.).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal