View Schedules

How do I open the Schedules tab?
  • Select
    View > Schedules
    , or click the
    Schedules
    button.
    TIP:
    You can also right-click an asset in the asset tree and select
    Schedules
    .
The
Schedules
tab shows the operations that are currently scheduled, whether these operations are active or not. An active Disaster Recovery schedule will run at its next scheduled time. An active Device Monitor schedule is running. An inactive schedule will run only on demand.
To view the
Schedules
tab, you must have
View a schedule
permission.
An asterisk (*) appears on the
Schedules
tab when any operation properties are modified for a schedule before the schedule is saved. If you close the
Schedules
tab without saving a modified schedule, you will be prompted to save any unsaved FactoryTalk AssetCentre data (including unsaved schedules and searches).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal