Create a schedule
Certain operations in FactoryTalk AssetCentre can be scheduled to run regularly at set intervals or at a specific time. If you create a schedule for a container, applicable devices in the container will automatically be added to the schedule. Any schedules you create are available for all FactoryTalk AssetCentre users in your system.
Prerequisites
- To create schedules, you must haveCreate a new schedule,Edit a schedule, andCommand a schedulepermissions.
To create a schedule
- SelectView > Schedules, or click theSchedulesbutton.
- Select the container or device (or asset) for which you want to schedule an operation. Only Rockwell Automation devices, ABB robots, Asset Inventory, custom devices, FactoryTalk Directory, FactoryTalk View Site Edition, FANUC robots, Generic FTP devices, Motoman robots, remote computers, and Siemens controllers can be included in Disaster Recovery schedules (if you have the correct activation).For all of a device's schedule properties to be available for modification, make sure each device to be added to a schedule has its Configuration Data defined in the device's properties. The Configuration Data will be used to specify the master file for a Disaster Recovery schedule.
- On theSchedulestab, click theNewbutton. (This button is only available if you have activation for the Disaster Recovery capability.)
- Complete theNew Schedule Wizard: Step 1 Schedule Propertiesdialog box and clickNext.
- Complete theNew Schedule Wizard: Step 2 Timing Propertiesdialog box and clickNext.
- Complete theNew Schedule Wizard: Step 3 Operation Propertiesdialog box and clickFinished.Allen-Bradley Logix 5000 Controllers in Change Detect schedules:If Change Detect Capable is blank or false in the controller asset'sPropertiesdialog box, then the controller is not shown here and cannot be added to the schedule.
Provide Feedback