Schedules toolbar and tab options
The following table shows the buttons on the
Schedules
toolbar, the Schedules
tab options, and their meanings.Toolbar button and tab options | Description |
|---|---|
![]() | Create a schedule. |
Delete | Delete the selected schedule. (The Active check box must be cleared to delete a schedule.) |
Properties | Modify timing properties of a schedule. (The Active check box must be cleared to modify timing properties.) |
![]() | Run the selected schedule immediately. (Not available for Device Monitor schedules.) |
Stop | Stop the selected running schedule. (Not available for Device Monitor schedules. To stop this type of schedule, clear the Active check box.) |
All Schedules | View all schedules created by all FactoryTalk AssetCentre users in your system. |
Filter by Schedules which include (device name) | View only those schedules in your FactoryTalk AssetCentre system in which the indicated device is included. |
Provide Feedback

Delete
Properties
Stop