Meanings of the bottom panes on the Schedules tab

Lower left pane
Use the left pane of the
Schedules
tab to view assets by location or by asset type. Also use this pane to select the assets that will participate in the schedule. When you create a schedule for a container, by default, all of that container's assets will participate in the schedule, except for assets that don't support that type of schedule. When you select an asset in this pane, the operation properties of that asset appear in the lower right pane of the
Schedules
tab.
While the schedule is running, status messages appear next to each asset.
Lower right pane
The lower right pane of the
Schedules
tab shows the properties of the asset selected in the lower left pane. Use this pane to set operation properties for assets included in the schedule. Assets included in the schedule contain set default operation properties. Once you modify an asset's operation properties, you can undo or save the new operation properties for the scheduled asset.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal