Delete an agent group
You can delete an agent group when needed.
To delete an agent group
- If you are not in it, enter Design mode.
- SelectView > Agent Groups, or click theAgent Groupsbutton.
- In theAgent group Creation and Agent Assignmentpane, select the agent group you want to delete.
- Click
on the Agent Group Creation and Agent Assignmenttoolbar or pressDelete.TIP:You can also right-click the agent group you want to delete and selectDelete. - When prompted to delete the agent group, clickYes.TIP:
- You cannot rename or delete the System Default agent group.
- You cannot delete a local or remote agent group that has one or more assets associated with it.
- If a local agent group has agent computers running or online, those local agent computers will be moved to the System Default agent group. However, a remote agent group cannot be deleted if any remote agent computers are online or active.
Provide Feedback