Rename an agent group
You can change the name of an agent group. This action is only available for a local agent group.
To rename an agent group
- If you are not in it, enter Design mode.
- On theMenubar, clickView > Agent Groups(or click theAgent Groupsbutton).
- In theAgent Group Creation and Agent Assignmentpane, right-click the agent group that you want to rename, and selectRenameor pressF2.
- Enter a new unique name, and click elsewhere or pressEnter.TIP:
- You cannot rename or delete the System Default agent group.
- You cannot rename the remote agent group because the remote group name is the FactoryTalk Directory server name.
Provide Feedback