Edit agent computer properties

You can change the properties of an agent computer in Agent Groups.
To edit agent computer properties
  1. If you are not in it, enter Design mode.
  2. On the
    Menu
    bar, click
    View > Agent Groups
    (or click the
    Agent Groups
    button).
  3. In the
    Agent Group Creation and Agent Assignment
    pane, select the agent computer you want to edit.
  4. Click Properties_button on the
    Agent Group Creation and Agent Assignment
    toolbar.
    TIP:
    You can also right-click the agent computer you want to edit and select
    Properties
    .
  5. Change the information as desired in the
    Agent Computer Properties
    dialog box and click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal