Create an agent computer

You can create an agent computer in Agent Groups to monitor the physical agent computers. The agent computer can be a local agent computer in a local FactoryTalk Directory to which the FactoryTalk AssetCentre system belongs or a remote agent computer in a remote FactoryTalk Directory.
TIP:
A local agent computer must be created within a local agent group. Similarly, a remote agent computer must be created within a remote agent group.
To create an agent computer
  1. If you are not in it, enter the design mode.
  2. On the
    Menu
    bar, click
    View > Agent Groups
    (or click the
    Agent Groups
    button).
  3. Select an agent group, or an agent computer under the group where you want to add the agent computer to. Otherwise, the agent computer will be created under the System Default agent group.
  4. Click add agent computer on the
    Agent Group Creation and Agent Assignment
    toolbar. The
    Add an Agent Computer
    dialog opens.
    TIP:
    You can also right-click the agent group and select
    Add Agent Computer
    .
  5. In the
    Add an Agent Computer
    dialog, enter the name, location and the description for the agent computer.
    You can click the
    Connect
    button to check whether the FactoryTalk AssetCentre Server service can connect to the agent computer.
  6. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal